• No : 21293
  • Release Date : 2018/08/22 16:26
  • Print

Auto tuning

After performing auto tuning, can I copy the motor constant in the setting value to another inverter and connect the same motor?
Category : 

Answer

Normally, the auto tuning condition depends on the combination of the inverter and motor (including wiring to the motor), perform auto tuning each time.
The parameter required for auto tuning can be used as is.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700