- No : 21333
- Release Date : 2018/08/22 16:27
-
Print
Brake resistor
Which terminal should be connected with the brake resistor? Should I remove the jumper of the terminals P and P1?
- Category :
-
Answer
Connect the brake resistor to the terminal P and terminal PR. (For the FR-A700-7.5K or lower, remove the jumper of the terminals PR and PX.)
Do not remove the jumper of terminals P and P1. (Remove the jumper of the terminals P and P1 when connecting the power factor improving DC reactor.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700