- No : 21339
- Release Date : 2018/08/22 16:27
-
Print
Input phase loss
An error "E.ILF" is displayed with the FR-E700.
Since it was an input phase loss error, I checked the power supply but the phase was not lost.
Are there any other possible causes?
- Category :
-
Answer
The FR-E700, D700, F700PJ may activate input phase loss protection "E.ILF" if the phase-to-phase voltage of the power supply has become largely unbalanced.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ