- No : 21351
- Release Date : 2018/08/22 16:27
- 
          
              Print
          
        
 
Offline auto tuning
    
      The instruction manual describes that "the motor capacity should be equal to or one rank lower than the inverter capacity". When performing offline auto tuning, can I use the inverter with capacity of 1.5K and the motor with capacity of 0.75 kW?
    
  
    - Category : 
- 
      
    
 
    Answer
  
    Auto tuning can be performed because the motor is one rank lower than the inverter capacity.
  
    
      
        - Product Name
- Inverter, magnet motor drive
        - Product Category
- Inverter
        - Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700