• No : 21353
  • Release Date : 2018/08/22 16:27
  • Print

Offline auto tuning

I performed offline auto tuning without running the motor, but I'm not sure if it succeeded. How can I check it?
Category : 

Answer

When auto tuning completes normally, the setting value of Pr.96 (Auto tuning setting/status) is changed to "3". When it is not changed, check the set parameter of auto tuning again.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700