• No : 21479
  • Release Date : 2018/08/22 16:27
  • Print

Support of Chinese

I received inquiry for exporting to China via a set manufacturer. One of the conditions is "Manuals written in Chinese should be available". Do you have manuals written in Chinese?
Category : 

Answer

Some types are designed for the Chinese market and provide Chinese manuals. (Note that the specifications of these types are partially different from the specifications for the Japanese market, there is no manual of the Japanese specifications products translated into Chinese.) The Chinese specifications products can be purchased in Japan. Contact your distributors or local office.
Product Name
Inverter, magnet motor drive
Product Category
Others
Series
FR-E700, FR-D700, FR-A700, FR-F700