- No : 21623
- Release Date : 2018/08/22 16:28
-
Print
Comparison of noise between FR-A100 and FR-A100E
Does the FR-A100E produce noise less than the FR-A100?
- Category :
-
Answer
The setting ranges of the carrier frequency are:
- FR-A100: 2 kHz to 14.5 kHz
- FR-A100EXCELLENT: 0.7 kHz to 14.5 kHz
The range of the FR-A100EXCELLENT is extended to the lower side, meaning that you can set the carrier frequency lower than the FR-A100. This means that noise can be reduced more than the FR-A100.
For the same carrier frequency, the noise levels are almost same.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A100