- No : 21635
- Release Date : 2018/08/22 16:28
-
Print
Difference from FREQROL-A200 (EXCELLENT) series
What are the differences from the FREQROL-A200 (EXCELLENT)?
- Category :
-
Answer
The following features are added to the FREQROL-A200 (EXCELLENT):
- PI control without an option
- Inverter electronic bypass sequenceThe following functions of the FREQROL-A200 (EXCELLENT) are not provided:
- Magnetic flux vector control
- Auto tuning
- Intelligent mode (shortest acceleration/deceleration, lift)
- Regenerative brake resistor (external installation is also not allowed)
- FR-EPA option installation
The permissible overload is reduced from the FREQROL-A200 (EXCELLENT). The size is reduced by one rank except for some capacities. The size is reduced by one rank except for some capacities.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A100