• No : 21690
  • Release Date : 2018/08/22 16:28
  • Print

Advanced magnetic flux vector control

While using Advanced magnetic flux vector control by setting Pr.80 (Motor capacity) and Pr.81 (Number of motor poles), the monitor frequency fluctuates. Can I eliminate slip compensation?
Category : 

Answer

Yes. Set Pr.89 (Speed control gain) to "0".
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700