- No : 21700
- Release Date : 2018/08/22 16:28
- 
          
              Print
          
        
 
FR-PA07
    
      When the optional FR-PA07 is connected, is the operation command source automatically transferred to the FR-PA07?
    
  
    - Category : 
- 
      
    
 
    Answer
  
    The operation command source is automatically transferred to the connected FR-PU07 or FR-PA07.
  
    
      
        - Product Name
- Inverter, magnet motor drive
        - Product Category
- Inverter
        - Series
- FR-E700, FR-D700, FR-F700PJ