• No : 21700
  • Release Date : 2018/08/22 16:28
  • Print

FR-PA07

When the optional FR-PA07 is connected, is the operation command source automatically transferred to the FR-PA07?
Category : 

Answer

The operation command source is automatically transferred to the connected FR-PU07 or FR-PA07.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ