• No : 21712
  • Release Date : 2018/08/22 16:29
  • Print

FR-A7AR E kit (Relay output function)

When using the optional FR-A7AR (Relay output function), can I set all of the three relay contacts to fault contacts? 
Category : 

Answer

Yes, you can set all of the three relay contacts to fault contacts.
Set Pr.320 (RA1 output selection), 321 (RA2 output selection), and 322 (RA3 output selection) to "99".
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700