- No : 21712
- Release Date : 2018/08/22 16:29
-
Print
FR-A7AR E kit (Relay output function)
When using the optional FR-A7AR (Relay output function), can I set all of the three relay contacts to fault contacts?
- Category :
-
Answer
Yes, you can set all of the three relay contacts to fault contacts.
Set Pr.320 (RA1 output selection), 321 (RA2 output selection), and 322 (RA3 output selection) to "99".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700