• No : 21722
  • Release Date : 2018/08/22 16:29
  • Print

Parameter setting

After clearing all parameters, I used the setting dial in the PU operation mode and pressed the SET key at 60 Hz. "60.00" and "F" alternately flickered alternately and I set the frequency to 60 Hz.
Then, I set Pr.2 (Minimum frequency) to "10 Hz", but the inverter did not operate.
The RUN LED blinks rapidly. What happened?
Category : 

Answer

Check if Pr.13 (Starting frequency) is set to higher than 10 Hz.

Also check if a signal is input through the terminal MRS.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ