- No : 21726
- Release Date : 2018/08/22 16:29
-
Print
Tuning
Although I set parameters for auto tuning, tuning was not performed and the motor rotated as usual.
How can I perform tuning?
- Category :
-
Answer
Check the parameters listed below necessary for tuning again.
Pr.9, Pr.71, Pr.80, Pr.81, Pr.83, Pr.84, and Pr.96
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700