- No : 21759
- Release Date : 2018/08/22 16:29
-
Print
NET mode
I want to use the CC-Link optional card FR-A7NC to implement CC-Link communication, but the inverter does not enter the NET mode.
I set Pr.340 (Communication startup mode selection) to "10", and Pr.79 (Operation mode) to "2".
What else should I do?
- Category :
-
Answer
After setting Pr.340 to "10", you need to power OFF then ON the inverter to make the new setting enabled because you are setting the operation upon power-on.
Power OFF then ON the inverter.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700