• No : 21813
  • Release Date : 2018/08/22 16:29
  • Print

Programmable controller

I use Mitsubishi Q series programmable controller and connect three inverters to it.
What happens if the inverter is not powered ON?
What happens if the inverter is then powered ON?
Category : 

Answer

The error LED on the master side of the programmable controller blinks (faulty station present).
According to the SW80 station information, an error flag is attached to information of the station to which the powered OFF inverter is connected. (Check it with the mater side of the programmable controller.)
When the inverter is powered ON, communications automatically start and another network is established. Error LED turns off.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700