- No : 21824
- Release Date : 2018/08/22 16:29
-
Print
CC-Link
In CC-Link operation, is it possible to monitor the running frequency and output current simultaneously?
- Category :
-
Answer
Yes. Set the first monitor code in the lower 8 bits and the second monitor code in the upper 8 bits of RWwn.
Set H6F to the first monitor code, and H70 to the second monitor code.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700