- No : 21840
- Release Date : 2018/08/22 16:29
-
Print
CC-Link
Is the program to set the operation mode described in the Instruction Manual of the FR-A7NC always necessary?
- Category :
-
Answer
If Pr.340 (Communication startup mode selection) and Pr.79 (Operation mode selection) are set so that the inverter starts CC-Link operation from power-on and does not switch to any other modes, this program is not necessary.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700