- No : 21870
- Release Date : 2018/08/22 16:29
-
Print
Operation mode, PU operation mode switching
After changing the parameter setting value, I tried to switch to the PU operation mode and I failed.
I use the FR-A7NC.
- Category :
-
Answer
Change Pr.340 (Communication startup mode selection) from "1" to "0".
Power OFF and then ON the inverter.
Operate the inverter according to the value of Pr.79 (Operation mode).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700