- No : 21879
- Release Date : 2018/08/22 16:29
- 
          
              Print
          
        
 
NET operation mode
    
      How should I set the inverter to start operation in the NET operation mode when it is powered on?
    
  
    - Category : 
- 
      
    
 
    Answer
  
    Set Pr.340 (Communication startup mode selection) to "1" or "2".
Also, by setting Pr.79 (Operation mode selection) to "0", "2", or "6", the inverter enters the NET mode when it is powered on.
  
    
      
        - Product Name
- Inverter, magnet motor drive
        - Product Category
- Inverter
        - Series
- FR-E700, FR-A700, FR-F700P, FR-F700