• No : 21879
  • Release Date : 2018/08/22 16:29
  • Print

NET operation mode

How should I set the inverter to start operation in the NET operation mode when it is powered on?
Category : 

Answer

Set Pr.340 (Communication startup mode selection) to "1" or "2".
Also, by setting Pr.79 (Operation mode selection) to "0", "2", or "6", the inverter enters the NET mode when it is powered on.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700