• No : 21881
  • Release Date : 2018/08/22 16:29
  • Print

Start command, speed command

Can I input the start command via CC-Link and speed command from the terminal 2 of the inverter?  
Category : 

Answer

You can do so by setting Pr.339 (Communication speed command source) = 1 (external).  
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700