• No : 21882
  • Release Date : 2018/08/22 16:29
  • Print

FR-Configurator

1. Can I set the station number with the USB connection?
2. Is the COM setting given by the FR Configurator necessary?
Category : 

Answer

1. You can set the station number.
However, you can only connect a single personal computer to a single inverter.
2. You can set communication by choosing Tool -> Option in the software.
The COM port setting is not necessary for USB connection.
You must specify a number for RS-232C connection.
Set the output COM port number.
(Check the port number in Device Manager on the personal computer.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700