- No : 21887
- Release Date : 2018/08/22 16:29
-
Print
CC-Link
Can I use the CC-Link option card FR-A7NC with other inverters?
- Category :
-
Answer
You can use it with the 700 series inverters. Note that the installation method of the card differs for the FR-E700 series and FR-A700/F700 series.
If you have purchased the standard FR-A7NC to use with the FR-E700, you can additionally purchase the FR-A7NC E kit cover only. Contact the distributor.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700