• No : 21888
  • Release Date : 2018/08/22 16:29
  • Print

CC-Link

I want to configure the inverter via communication using the FR-A7NC.
Is it no longer necessary to wire the external terminals of the inverter if I use this option?
Category : 

Answer

When configuring the inverter via communication such as CC-Link, some signals still requires to be input from the external terminals.
(Terminal OH: External thermal relay input and others)
If you need any of these signals, you still need cabling the external terminals.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700