• No : 21899
  • Release Date : 2018/08/22 16:29
  • Print

CC-Link

Can I send operation commands (forward/reverse) and set parameters via CC-Link?
Category : 

Answer

Yes.
You can issue operation (forward/reverse), frequency setting, parameter read/write, and operation monitor commands.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700