• No : 21900
  • Release Date : 2018/08/22 16:29
  • Print

CC-Link

When operating the inverter via CC-Link, is it necessary to input analog and multi-speed signals from an external source?
Or, can I just input numeric data in words?
Category : 

Answer

If you are using CC-Link just to monitor the inverter and using the analog signal and multi-speed setting to set the frequency, you need to input them externally.
If you are using CC-Link to set the frequency, external signals are not necessary.
You can directly write numeric values to the remote register to operate the inverter.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700