• No : 21901
  • Release Date : 2018/08/22 16:29
  • Print

CC-Link

I am considering to control the inverter with the output module and DA conversion unit of the programmable controller using CC-Link. To what extent can I control them from CC-Link communication using the optional FR-A7NC (E kit)?  
Category : 

Answer

You can start/stop operation, set the frequency, read/write parameters, and monitor the inverter via CC-Link communication.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700