• No : 21902
  • Release Date : 2018/08/22 16:30
  • Print

CC-Link

Should I purchase the FR-A7NC option to implement CC-Link communication?
Category : 

Answer

Purchase the FR-A7NC if you are using the option with the FR-A700 or FR-F700P (F700).
Purchase the FR-A7NC E kit if you are using the option with the FR-E700.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700