• No : 22255
  • Release Date : 2018/08/30 13:48
  • Print

How to use the "S/S" terminal

Answer

The "S/S" terminal is used to switch the input type (sink input and source input).

For the source input, connect the "S/S" terminal to the "0V" terminal, and short-circuit between the "24V" terminal and the "- input terminal: X□□□" to turn on the input.
For the sink input, connect the "S/S" terminal to the "24V" terminal, and short-circuit between the "0V" terminal and the "- input terminal: X□□□" to turn on the input.
Product Name
FX1S, FX1N, FX1NC, FX2N, FX2NC, FX3S, FX3G, FX3GC, FX3U, FX3UC
Product Category
Main unit, I/O Extension
Series
MELSEC-F series