• No : 22273
  • Release Date : 2018/08/30 13:48
  • Print

Communications using the built-in USB port of the FX3 series

Connection is not established when the built-in USB port of the FX3 series(FX3S/FX3G/FX3GC) is connected to a personal computer(engineering tool).
Category : 

Answer

When you connect the built-in USB port of the FX3 series to the personal computer for the first time, you need to install the USB driver into the personal computer.

The installer is in the USBDriver folder which can be found under the Easysocket folder (in a folder used to install GX Developer or GX Works2).
Product Name
FX3S, FX3G, FX3GC
Product Category
Main Unit, Network/Communications, Engineering Software, GX Developper, GX Works2
Series
FX3S, FX3G, FX3GC