- No : 22275
- Release Date : 2018/08/30 13:48
-
Print
Turning on a bit in the data register
Is it possible to turn on a bit in the data register?
- Category :
-
Answer
In the FX3U/FX3UC series, the bit specification of the data register is possible.
(Example) D0.7→7th bit in D0
For the other types of MELSEC-F programmable controllers, transfer the bit device information to the data register by using the MOV instruction.
- Product Name
- FX1S, FX1N, FX1NC, FX2N, FX2NC, FX3S, FX3G, FX3GC, FX3U, FX3UC
- Product Category
- Main unit, Engineering Software, GX Developper, GX Works2
- Series
- MELSEC-F series