• No : 22275
  • Release Date : 2018/08/30 13:48
  • Print

Turning on a bit in the data register

Answer

In the FX3U/FX3UC series, the bit specification of the data register is possible.
(Example) D0.7→7th bit in D0

For the other types of MELSEC-F programmable controllers, transfer the bit device information to the data register by using the MOV instruction.
Product Name
FX1S, FX1N, FX1NC, FX2N, FX2NC, FX3S, FX3G, FX3GC, FX3U, FX3UC
Product Category
Main unit, Engineering Software, GX Developper, GX Works2
Series
MELSEC-F series