• No : 23569
  • Release Date : 2018/09/14 15:09
  • Print

Acceleration/deceleration time change

Can I change the acceleration/deceleration time during operation?
Category : 

Answer

Yes, the time can be changed during operation by using the acceleration/deceleration time change function.
Set the acceleration/deceleration time change parameter of the servo data and the command generation axis parameters, and execute the following speed change instruction.
(1) Motion SFC program
    Speed change request CHGV, CHGVS
(2) Sequence program
    Speed change request M(P).CHGV, D(P).CHGV, M(P).CHGVS, D(P).CHGVS
Product Name
Motion controller
Series
MELSEC iQ-R