• No : 23577
  • Release Date : 2018/09/14 15:09
  • Print

Error 2035

Answer

Error 2035 (Command frequency error) occurs when the servo amplifier detects a command frequency error.
(1) When the command is the permissible speed or higher. Check operation pattern.
(2) When the command is lower than the permissible speed.
    • Take countermeasure against I/O signal noise
    • Take countermeasure against servo system controller noise

Refer to relevant servo amplifier manuals for details.
Product Name
Motion controller
Series
MELSEC-Q