- No : 23603
 
      - Release Date : 2018/09/14 15:09
 
        - 
          
              Print
          
        
 
  
 
Parameter initialization
    
      How do I initialize the parameters?
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    The following shows the initialization procedure.
(1) Turn OFF the PLC ready flag.
(2) Turn ON "[Cd.2] Parameter initialization request".
    Set "1" to the buffer memory 1901. After the completion of initialization, "0" is automatically set to the buffer memory 1901.
(3) Reset the PLC CPU, or turn the power OFF to ON.
  
    
      
        - Product Name
 
          - Simple Motion module
 
      
      
        - Series
 
          - MELSEC iQ-R
MELSEC iQ-F