FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Counting of a built-in high-speed counter
Back
No : 24787
Release Date : 2019/02/28 09:06
Print
Counting of a built-in high-speed counter
When a built-in high-speed counter does not start counting, what are the possible causes?
Category :
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
Engineering Software
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Main Unit
Answer
Check that the RST instruction of the high-speed counter is not executed while the program is running.
For the high-speed counter which supports the external reset input, check that the external reset input is not on.
Product Name
FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Product Category
Main unit, Engineering Software, GX Works2, GX Developer
Series
MELSEC-F series