• No : 44965
  • Release Date : 2025/05/08 09:06
  • Update : 2025/11/05 08:03
  • Print

Regarding connectable I/O Modules

Which I/O Modules can be connected to the MX-F Model?

Category : 

Answer

It is possible to connect the I/O Module of the MX-F Model to the extension cable type I/O Module of the iQ-F series. 

To connect an extension cable type I/O Module of the iQ-F series, you need a connector conversion Module: FX5-CNV-IFC or an Extension power supply module: FX5-C1PS-5V.

MX-F Model I/O Module List

iQ-F Series I/O Module List

Product Name
MX-F Model
Series
MELSEC MX Controller