• No : 44966
  • Release Date : 2025/05/08 09:05
  • Print

Regarding number of expansion adapter connections

How many expansion adapters can be connected to an MX-F Model?

Category : 

Answer

The number of expansion adapters varies depending on the type of adapter, and up to six can be connected.
・Analog adapter: Up to 4
・Communication adapter: Up to 2

Product Name
MX-F Model
Series
MELSEC MX Controller