• No : 44969
  • Release Date : 2025/05/08 09:05
  • Print

Regarding built-in ethernet port differences

The MX-F model has 2 built-in Ethernet ports. Is there any difference?

Category : 

Answer

Port 1 becomes the CC-Link IE TSN, and port 2 can be switched between Ethernet and CC-Link IE TSN.
To use port 2 as an Ethernet port, set the Built-in Network Type to "Ethernet + CC-Link IE TSN" when creating a new project in GX Works3.

To use port 2 as the CC-Link IE TSN port, set the Built-in Network Type to "CC-Link IE TSN" when creating a new project in GX Works3.

To switch Port 2 while creating a project, select [Project] ⇒ [Change Module Type/Operation Mode] in GX Works3 and select [Built-in Network Type].

Product Name
MX-F Model
Series
MELSEC MX Controller