• No : 44973
  • Release Date : 2025/05/08 09:08
  • Update : 2025/10/31 15:18
  • Print

Regarding maximum number of connected stations for built-in CC-Link IE TSN

What is the maximum number of connected stations for the built-in CC-Link IE TSN of MX-F Model?

Category : 

Answer

The maximum number of stations that can be connected in the network depends on the model name of the MX-F model.
・MXF100-16 N32/P32: Up to 46 stations
・MXF100-8 N32/P32: Up to 38 stations

Product Name
MX-F Model
Series
MELSEC MX Controller