• No : 44983
  • Release Date : 2025/05/08 09:06
  • Update : 2025/11/05 08:05
  • Print

Regarding connectable Intelligent Function modules

Which intelligent Modules can be connected to an MX-F Model?

Category : 

Answer

The MX-F Model can be connected to the intelligent function modules of the iQ-F series. 

Connectable intelligent function modules are shown below.

Product Name
MX-F Model
Series
MELSEC MX Controller