Motion module: Is the Mark detection function used in the FX5 40/80SSC-G compatible with the built-in motion function of the MX-F Model?
The Mark detection function of the FX5-40/80SSC-G is supported by the Touch probe function of the MX-F Model.