- No : 23577
- Release Date : 2018/09/14 15:09
- 
          
              Print
          
        
 
Error 2035
    
      What is error 2035?
What should I do when it occurs?
    
  
    - Category : 
- 
      
    
 
    Answer
  
    Error 2035 (Command frequency error) occurs when the servo amplifier detects a command frequency error.
(1) When the command is the permissible speed or higher. Check operation pattern.
(2) When the command is lower than the permissible speed.
    • Take countermeasure against I/O signal noise
    • Take countermeasure against servo system controller noise
Refer to relevant servo amplifier manuals for details.
  
    
      
        - Product Name
- Motion controller
        - Series
- MELSEC-Q