FAQ


FAQAbout Products
- FAQ > Drive Products > Geared Motors > Geared Motors Parallel shaft type > About China CCC certification
FAQ
About China CCC certification
Has the GM-J2 series received CCC certification?
Answer
We have not acquired China's CCC certification for the GM-J2 series.
"Small-power motors" are among the products covered by China's CCC certifications (GB12350-2009), these are motors of 1.1kW or lower. The GM-S, D, SHY, and SSY series have been certified for the 0.1 to 0.75kW range.
"Small-power motors" are among the products covered by China's CCC certifications (GB12350-2009), these are motors of 1.1kW or lower. The GM-S, D, SHY, and SSY series have been certified for the 0.1 to 0.75kW range.
- Product Name
- Geared Motors
- Series
- Geared Motors Parallel shaft type, Geared Motors Right angle shaft type