FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Frequency setting by the CC-Link
FAQ
Frequency setting by the CC-Link
When the frequency is set via the CC-Link, is the frequency setting value set with the PU (operation panel) changed?
- Category :
Answer
When the frequency setting value is written by the CC-Link to EEPROM, the frequency setting value set with the PU (operation panel) is changed.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800, FR-E700, FR-E700EX