FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > PLC function
FAQ
PLC function
On what condition does the PLC function device: SM1217 turn ON?
- Category :
Answer
Vector control: The SM1217 turns ON when the motor rotates even if no forward rotation command is send. Other than vector control: The SM1217 turn ON by forward rotation + RUN (output frequency).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800