FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A800-R2R
FAQ
FR-A800-R2R
Is Real sensorless vector control available?
- Category :
Answer
Yes, it is. However, it is not suitable for the low speed regenerative side. It is also recommended to use a dedicated control for winding/unwinding applications that require accuracy. (dancer feedback speed control, tension sensor feedback speed control, tension sensorless torque control, and tension sensor feedback torque control)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800 Plus