FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > FR-A701
FAQ
FR-A701
Can I connect the reactor for the harmonic suppression to the FR-A701?
- Category :
Answer
The AC reactor (FR-HAL) is built in the FR-A701. (The circuit type in the Harmonic Suppression Guidelines is three-phase bridge (capacitor smoothed), with reactor (AC side).) The connection with the stand-alone option AC reactor (FR-HAL) is not required. The DC reactor (FR-HEL) cannot be connected.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A701